SSM2603: FAQ
When booting the SSM2603 and SSM2604, a control register programming sequence must be followed:
CONTROL REGISTER SEQUENCING
1. Enable all of the necessary power management bits of Register R6 with the exception of the out bit (Bit D4). The out bit should…
Hi!
I try to use the SSM2603 chip on Zybo Z10 board for a month now and I still have the same problem: if I try to play a sinewave, the output signal look like that: (blue=right, yellow:left)
I triple check everything:
-My i2s input signal is OK, two's complement…
I just purchased a EVAL-SSM2603 and I can't find a windows 10 driver that will work with the USBi.
Is there a driver that will support USBi device on windows 10?
Hi all,
Title says it all. Thank you.
Regards
Mark
Can the SSM2603 serve as a functional replacement for the max9860 if used with the max98307 amplifier?
We are concerned about the output load impedance between these two chips.
Max98307 has 8 ohm input load, ssm2603 has 16 ohm output load. Is that a problem…
Hello,
I am missing some specifications in the ssm2603 datasheet,
that is: maximum low input and minimum high input voltage, as well as output drive capability (max output low voltage) for the I²C pins of this device.
Regards,
Robert Larice
…we just got the SSM2603 Evaluation Board, when we connect with the computer, the USB devices cannot be identified. I found that the USB drivers is X86 , it is that mean the computer operating system is 86 bits? My computer operating system is 64 bits.…