• Can you provide Residual Phase Noise Data for ADL5545?

    I am using ADL5545 in synthesizer design. Please provide Residual Phase Noise Data for ADL5545?

  • RE: FAQ: Residual Phase Noise of ADL5544

    I am planning to use ADL5544 for 100MHz frequency. What will be the Residual Phase Noise for 100MHz frequency?

    Will it be same as above or will it improve?

  • RE: Additive/Residual Phase Noise Graphs for "Low Phase Noise" Amplifiers like ADPA9002, HMC5805A

    For most of the devices listed in the table, you can find plots of residual phase noise on Engineerzone. Do a general search on residual phase noise. See link below. 

    https://ez.analog.com/search?q=residual%20phase%20noise&group=116

  • HMC313 Residual Phase Noise

    Hi Application team,

    Is it possible to provide Residual Phase Noise for HMC313 ?

    My customer is using HMC311LP3 but would like change to HMC313 for better reverse isolation.

    The residual phase noise of HMC311LP3 is in the selection table, but I couldn…

  • RE: FAQ: Residual Phase Noise of HMC465LP5

    A: Figure 1 below shows the residual phase noise of HMC465LP5 measured at  an output power of 22 dBm (Pin = 9 dBm).  Figure 2 shows the baseline phase noise of the measurement setup.  At carrier offset frequencies below 1KHz, the measurement is dominated…

  • RE: FAQ: HMC441LP3E Residual Phase Noise

    A: Figure 1 shows the residual phase noise of HMC441LP3E, measured at an output power of 16 dBm at 8 GHz. Figure 2 shows the baseline phase noise of the measurement setup.

    Figure 1. HMC441LP3E Residual Phase Noise, Pout = 16 dBm @ 8 GHz.

    Figure 2…

  • RE: FAQ: Residual Phase Noise of ADL5521

    A:

    Figure 1 shows the residual phase noise of ADL5521, measured at an output power of 21 dBm ( PIN = 4.3 dBm) at 2 GHz. Figure 2 shows the baseline phase noise of the measurement setup.  At carrier offset frequencies below 1 KHz, the measurement is dominated…

  • RE: FAQ: Residual Phase Noise of HMC311S

    A:

    Figure 1 shows the residual phase noise of HMC311S, measured at an output power of 15.3 dBm ( PIN = -1 dBm) at 2 GHz. Figure 2 shows the baseline phase noise of the measurement setup.  At carrier offset frequencies below 1 KHz, the measurement is dominated…

  • RE: FAQ: Residual Phase Noise of HMC589A

    A:

    Figure 1 shows the residual phase noise of HMC589A, measured at an output power of 18.5 dBm (PIN = 0 dBm) at 2 GHz. Figure 2 shows the baseline phase noise of the measurement setup.  At carrier offset frequencies below 1 KHz, the measurement is dominated…

  • Residual phase noise of HMC575 and HMC573

    The datasheets of the HMC575 and HMC573 frequency doublers only give residual phase noise at 100 kHz offset. Can you perhaps provide a graph over a wider offset frequency range?

    Thanks.