• OP16: Slew rate

    Does the OP16 op-amp slew rate response fall as the differential signal falls?
    (ie diff signals below 50mV). Do you have a graph for this?

     

    The slew rate for the device is 25V / us, for a Closed loop gain of 1 and Model
    N, with +-15V power supplies…

  • OP15/OP16/OP17 part alternative

    I am having an old instrument which uses OP 15 and OP 16 IC's, lately, in the instrument, these ics have gone bad. The AD sites show these parts are obsolete. What is the pin to pin replacement of these ICS' or some better IC's with similar specifications…

  • ADN4605 Design Support Files

    Attached and linked are files supporting the development of systems using the ADN4605, 4.25Gbps 40x40 Digital Crosspoint Switch.

    We recommend that, if you download and use this document, you subscribe to email notifications for either the entire forum…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • ADN4605 channel status registers

    I am able to access ADN4605 device and can access all the registers. But all the channel registers are showing 0x3F. I did not understand this issue? Is it software or Hardware issue?

    i2c write at address 0x0 data 0x1

    i2c write at address 0x0 data …

  • ADI运算放大器选型指南

    ADI运算放大器选型指南