• RE: LTC4015 is burning

    Hello,

    I don't see M4 or M5 in your schematic. It is likely an inrush issue. Please refer to the attached guide.

     PDF

    Regards,

    Zack

  • Hardware Configuration Register Blocks- Data associated with Addresses is inconsistant

    Hello,

    I want to note the address and data associated with the changes (toggle values) I make in the register control window

    and use it with an external uC to control various settings in my program.

    I am having issues knowing the data associated with…

  • RE: adv7391

    Hi,

     I beleive,Spartan-3 code will not be available on public forum.Please contact your local FAE or salesrep. They will route to the appropriate person.

     To compare your video output,directly connect the source to sink and take that output as your reference…

  • RE: PDCLK problem of EVAL-AD9957

    Thanks for your reply!

    Yes, my PDCLK pin has no expected signal in QDUC mode. In my QDUC mode, the PDCLK pin is always logic low, despite the fact that the PDCLK enable bit has been set as logic high. My control words are as follows (I use the crystal…

  • FAQ: ADIS16445 Mechanical Design Tools

    Q:

    Do you have a 3-D model file for the ADIS16445?

    -----------------------------------------------------------------------

    A:

    Yes, we have a 3-D model for this product, in the form of a .STEP file.  While we are not experts on all 3-D rendering programs…

  • 请问AD9910能否输出三角波、锯齿波和方波?

    您好,

      我想用AD9910的DRG模式输出三角波和锯齿波,请问是否可以实现。

      我按照个人理解配置了一些寄存器,发现输出波形在y=0附近仍然有很严重的正弦调制,请问是否能输出完全规整的三角波和锯齿波呢?

      按照个人理解,DRG模式下,控制DRHOLD引脚即能输出方波,此时的频率信息是否也需要非常精确的对应呢?

      下面是我当前用于输出三角波的寄存器配置:

       01:0x006E 0820

         02:  0x183F C000

         0E:  0x3FFF 0000 0002 0000

         0B…

  • AD9880/AD9380/AD9381/AD9398/AD9393 Design Support Files

    Attached and linked are several files supporting the development of systems using the AD9880, AD9380, AD9381, AD9398, and AD9393 video Rx products.

    File Content
    PRODUCT SUPPORT
    AD9880…
  • 2010-05-06 04:40:45     BUG: scheduling while atomic...

    2010-05-06 04:40:45     BUG: scheduling while atomic...

    Pavel Frolov (BELARUS)

    Message: 89172   

    I've got kernel crash after 10-30 min. Do you have any ideas why it occurs.

    My kernel: 2009R1.1-RC1, Processor bf526.

    eth0: hw csum failure.

    Hardware…

  • [#4758] Exception dumping starves watchdog

    [#4758] Exception dumping starves watchdog

    Submitted By: Jie Zhang

    Open Date

    2008-12-29 02:30:05    

    Priority:

    Medium     Assignee:

    Nobody

    Status:

    Open     Fixed In Release:

    N/A

    Found In Release:

    2008R1.5-RC3     Release:

    Category:

    N/A     Board:

    N/A