• LTC6993-1 OUTPUT waveform abnormal phenomenon

    The input signal and output signal are different from the expected signal. What is the reason

    Red signal - Input / Yellow signal - Output

  • RE: LTC6993-1 TRIG pin specifications and connections

    The TRIG input pin on the LTC6993-1 is a simple CMOS logic input with voltage hysteresis to accommodate slow slewing input signals. The large capacitor on the pin will limit the slew rate of the TRIG input signal but should not cause any problems. For…

  • LTC6993

    I am using an LTC6993-3 timer chip and I am using it to generate a positive output pulse of approximately 27 seconds.  It is triggered from a high to low transition on the trigger pin and this transition is produced by a comparator.  This device is non…

  • The minimum pulse width of LTC6993 (monostable pulse generator)

    Hi ADI engineer,

    I am trying to use LTC6933-2 as the one-shot generator and thus I want to know the minimum value of pulse width I can get in real case.

    According to the datasheet, the pulse width range is larger than 1us and the programmable tout is…

  • wants to confirm whether LT8708-1 (LT8708EUHG-1#PBF) can work independently.

    The LT8708EUHG-1#PBF specification shows that the LT8708-1 always operates as a slave to the master LT8708, Mainly used in parallel with LT8708, At present, our customer wants to use LT8708-1 (LT8708EUHG-1#PBF) separately without parallel connection.…

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…

  • Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…

  • ADATE305 VDDO_0/1, VSSO_0/1 termination

    Hello,

    In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?

    Best Regards,

  • Can LT8708EUHG-1 be used as a standalone DC-DC?Can LT8708EUHG-1 be used as a standalone DC-DC?

    Can LT8708EUHG-1 be used as a standalone DC-DC? Can LT8708EUHG-1 be used alone? Can LT8708EUHG-1 work alone?