Hi,
I would like to use ADUX1020.
So, I have two questions. Please help me.
Question1:
I would like to use six ADUX 1020 and control them with one master.Can I set and distinguish slave addresses to each sensor with I2C communication?
In the…
Hi all,I would like to ask about ADUX 1020.
Using the Optical Gesture Evaluation Tool,I'm evaluating ADUX1020-EVAL-SDP(EVAL-SDP-CB1Z and ADUX1020 MCM board).
I checked the graph of ”Y Ratio vs. X Ratio” on the Graph XYI tab.
Even if I move…
How do I connect an external LED to the ADUX 1020 eval board? Is there a place on the board that allows me to access the LEDX pin? Also, would I need to disable the onboard LED?
Thanks,
Nathan
.如果要更改AD637 均方根统计的时间是更改Cav的值吗?Datasheet上说明的好像是25ms/UF,需要统计信号频率不超过700Hz。我看AD637的应用中都是固定的Cav,不知到底能不能改。
Did you refer to the formula in "section2.pdf" page 18 in the link "RMS to DC Conversion Application Guide..." in the datasheet?
It states that for two pole output filter like your setup, The 1% settling time is equal to
Dear Sir/Madam,
I just use your AD637 RMS to DC converter.Input is the sound signal.CAV is put 100uF capacitor.When the large sound is inputed to AD637 Vin momentarily,we just found to output pulse-signal.So the analog meter that is put the RMSOUT-pin…
Hi
I want to know when ADV8005 memory mode is set to YCbCr-12b-10b-10b
And HDMI TX color depth is set to 30bit, (10bit x 3)
What is the max output level will be? 1020 or 1023?
It seems the max value is force to 1020?
I try to use contrast to set to…
图片是手机拍的 我把反馈电容CAV由10uF换成了0.1uF 波形变成如下图所示 还是有失真