Hello,
After using the ADSP-2191M for 15+ years we're looking for a new processor, mostly because VisualDSP++ 3.5 is not supported on current operating systems.
We're interested in a more recent processor that supports fixed-point arithmetic, has…
Hi,
we have a system with ADSP-2191M that starts in bypass mode (BYPASS pin unconnected). After successful start the program sets PLLCNTL to required multiplication factor (CLKIN=40MHz, multiplier=4x to achieve 160MHz CCLK) and switches CCLK to be driven…
Hi Tingting,
The internal ROM is not user programmable. It is factory programmed, it requires a minimum order and there is an NRE associated for custom ROM programmed parts. For further details please contact your local sales representative.
Best regards…
FFT Accelerator on ADSP-SC58x/ADSP-2158x is a completely new design as compared to the FFT accelerator on ADSP-214xx processors. The major differences/features of the FFT accelerator on ADSPSC58x/ADSP-2158x are:
Customer ask some questions.
Right now we have plenty of software for ADSP-21489, but it’s quite hard to port it to ADSP-SC573 family. Code itself
is 99% C and C++.
Does family ADSP-SC573 have interface with external static memory like AMI for ADSP…
The FIR accelerator on ADSP-SC58x/ADSP-2158x works exactly in the same manner except the following differences:
→ Unlike in ADSP-214xx, you don't need to enable the FIR accelerator in PMCTL1 register explicitly in ADSP-SC58x/ADSP-2158x. In fact,…
The IIR accelerator on ADSP-SC58x/ADSP-2158x works exactly in the same manner except the following differences: