• ADSP- 2189M

    Hi  ,

    Has anybody come across this DSP device. I cannot find much material on the internet. For example any example source codes. I have a project GPS module date is coming wrong as an input to this DSP device. The DSP device needs to be programed to correct…

  • RE: WSMS on ADSP-2189M

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADSP-2189M SPORT hardware companding

    We're using the ADSP-2189M DSP, and specifically the hardware u-law/A-law companding on the SPORTs.

    ITU-T G.711 specifies u-law and A-law to work on "integer samples", with reduced sample widths (13 magnitude bits for u-law, 12 for A-law).…

  • How can I get an evaluation license or permanent license for VDSP++ 3.5?

    I have a 218x EZ-ICE and 2189M EZ-LITE eval board, but need a license to get the system running.

  • OS and vdsp 3.5

    what is the most advanced windows OS these tools can run on?

    customer doing 2189M,N development and wants to do that for 10 years.  now the question is the OS. 

    thanks,

    tim

  • RE: Wanted ADSP 2181 EZ-Kit Lite - Help

    Hi Dave,

    The 2181 EZ-Kit was not transitioned to be RoHS compliant and was made obsolete a number of years ago. For further information on RoHS compliancy and a list of tools which were not transitioned have a look at the following FAQ: FAQ:  What is…

  • TAGS LIST: Processors & DSP

    ADUC812
    ADUC814
    ADUC816
    ADUC824
    ADUC831
    ADUC832
    ADUC834
    ADUC836
    ADUC841
    ADUC842
    ADUC843
    ADUC845
    ADUC847
    ADUC848
    ADUC7019
    ADUC7020
    ADUC7021
    ADUC7022
    ADUC7023
    ADUC7024
    ADUC7025
    ADUC7026
    ADUC7027
    ADUC…
  • RE: ADSP-218x LDF file that supports overlays

    Hi,

    EE-100 is a pretty old engineer note. While a lot of the information is still relevant, the Linker version 2.3 it refers to was a patch for VisualDSP++ 2.0. The Linker in VisualDSP++ 3.5 October 2006 Update (v3.4.1.5) supports overlays fully.

    Have…

  • RE: ADSP2189M EZ-KIT LITE Drivers

    Hi Elio,

    Great, I'm glad you have been able to connect. I'm not certain what could be causing this issue, however it sounds possible that the code being loaded is overwriting the monitor program. When you say you are loading the examples, do you meant…

  • RE: How to use the directives .swf_on and .swf_off?

    The Shadow Write FIFO anomaly only affected early silicon revisions of the ADSP-21160 and ADSP-21161 parts. The anomaly sheets for ADSP-21479 and ADSP-21489 are at the links below:

    https://www.analog.com/media/en/dsp-documentation/integrated-circuit-anomalies…