• RE: ADSP-2181 Obsoleted

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Wanted ADSP 2181 EZ-Kit Lite - Help

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Wanted ADSP 2181 EZ-Kit Lite - Help

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Is there a conflict between the host and ADSP-2181 to read internal PM using the IDMA port

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADSP-2181 based Development Setup

    Dear Klaus,

    Thanks for your reply.

    I found some source code. Source code files are having extension of *.dsp. The project file, I can open in VDSP3.5

    The code seems to be in Assembly Language. Here is part of the source code.

    #include <def2181.h…

  • HOW ADSP-21489 MEMORY SELECT PINS MS0-MS1-MS2-MS3 WORKS ?

    Hello,

    I have ADSP-21489-EZ-KIT development. My question is about using parallel FLASH = FLASH_CS\ = MS1\ pins.
    1-) MS1\ pin used for parallel flash chip select. How can I change it to MS2\ (or MS0\ or MS\3)  pin on my own board ?
    2-) When I was using…
  • RE: ADSP 2181 processor stops execution of main routine

    Hi Victor,

      Apologies for the delay in the response.If I understand your situation correctly, Prototype board functions correctly. Out of 9 new board which are based on prototype board, 4 boards works correctly. In the 5 failing boards, ADSP-2181 processor…

  • RE: VisualDSP3.5 & 2181 EZKIT

    Here is the video reply to this thread on youtube. Of course it is blocked by ADI, but you can choose to continue to see the video anyway, even through they really go out of their way, to try to block it...

    VisualDSP++ 3.5 elf2aexe crippled executables…

  • ADSP-2181-133 Firmware Using Visual DSP ++ 3.5

    Hi All,

    I am worki ng no one of Redesign Project. Originally the project was developed in 1998 based on ADSP-2181BSZ-133.

    The firmware was written in some unknown command line development environment.

    Now I tried to port that firmware on Visual DSP…

  • ADSP-21363BSQZ

    What is difference between

    ADSP-21363BSQZ and

    ADSP-21363BSWZ ?