Hi,
Any one can help me, how to read OSF(Original Sampling Frequency) from the ADAV801 Consumer Audio Standard. As per the IEC 60958 standard we can read the OSF from the Register address 0x24 (bits 36 - 39). but in the ADAV801 Codec Chip those Bits…
at present i am working with a ADAV801-based CODEC-board, which works fine and is easy to handle by setting the approriate registers.
In addition now i want to use the ALC-function of the ADAV801 because the ADC Input level is not well defined …
Hi, We are using BF-533 Ez-kit Lite along Audio extender card for our application. System Usage: Ø We are giving digital input and playing back using analog o/p. Ø The digital i/p is received using ADAV801 and played back using AD1938. Ø The sysclk3 of…
Hello,
a question regarding the SYSCLK2 output on ADAV801.
At XIN I have a 27MHz crystal, at SYSCLK2 I need 24.576 MHz with 50% duty cycle.
Because I use PLL2 and double sample rate (48 kHz x 2), I need to write in register 0x75 the value 0x10.
I am attempting to add ADAV801 codec support to my 2.6.35 kernel to beused with an ARM processor. I can see that there is a mainlinedadav80x.c driver that appears at kernel version 3.1, I have had aquick look at back-porting the driver but this looks…
I have an EVAL-ADAV803 board which I am trying to connect to a Atmel AT91SAM development board, with Linux, via I2C and I2S. I have the kernel module loaded on the AT91 and I would like to prevent the CPLD from connecting to the ADAV803. How can I do…
Is there a way to determine the incoming SPDIF sample rate with the ADAV801?
does anyone have experience with the suitable settings of the ADAV801 ALC Control registers (recovery mode, attack time, release time etc) for a acceptable speech regulation ?
Kind regards
Christian
Hello,if I use these settings (please see attachment for more information), I measure a LRCLK of 96 kS/s on the I2S interface at the serial output port, but we need 192 kS/s . Which register settings would be necessary for it? If I put a 192 kHz SP…
in our application, we want to output either 48, 96 or 192 kHz SPDIF.
The audio data coming in via I2S and we must, depending on the sampling rate change the channel status information. In case of sampling frequencies 96 and 192 kHz copying from…