• TMP37 FIT Rate

    Hi All,

    What are FIT Rates (60% and 90%) of the TMP37?  Same as those of TMP36?

    Regards,

    Kazu

  • Is TMP37 temperature sensor sensitive to switching transients and noise?.

    Is TMP37 sensitive to switching transients and noise from DC-DC power converter?. If TMP37 is powered through DC-DC converter it doesnt work whereas if it is powered through an external power supply it works. I dont know what causes this issue. Please…

  • RE: What does the Offset Voltage refer to with TMP36

    For TMP36 it just means that in order to convert voltage into temperature, simply use the basic formula:

    Temp in °C = [(Vout in mV) - 500] / 10

     

    So for example, if Vout is 1V that means that the temperature is ((1000 mV - 500) / 10) = 50 °C

    Compared…

  • TAGS LIST: Sensors & MEMS

    ADXL78
    ADXL001
    ADXL278
    ADIS16223
    ADIS16240
    ADIS16209
    ADIS16203
    ADIS16201
    ADXL193
    ADISEVAL
    ADXL1005
    ADIS16000
    ADIS16210
    ADIS16227
    ADIS16228
    ADIS16229
    ADIS16305
    ADXL1001
    ADXL1002
    ADXL1004
    ADXL103
    ADXL151
    A…
  • tmp36 conversion formula or accuracy?

    Hi ( warning newbie! )

    Im running thru the Arduino starter kit stuff and they include a TMP36 to do some temperature sensing on their starter projects...

    I was able to get very accurate middle wire voltage readings from the Arduino ADC - that match…

  • tmp36 adhesion

    Hi,

    I am trying to decide whether to use glue or tape to stick the tmp36 temp sensor to metal and plexi glass for a research project.  The glue or tape must be thermally conductive, but electrically non conductive.  Cost and functionality are my two main…