• RE: SSM3302

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: SSM3302 help

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: SSM3302 Demodulation Filter

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: SSM3302 Output filtering

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: SSM3302 to drive 3ohm 3.5W speaker in mono mode

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • SSM3302 - TEST pins

    Hello

    How to connect TEST pins?

    Datasheet says to connect to ground - kit guide UG-360 says to connect to AVDD using pullup 4.99K resistors.

    thx

  • SSM3302 mono mode what is corect output connection?

    Hello.

    What is correct PBTL output mode connection, from datasheet or UG-360?

    I think that proper connection are LOUT+//ROUT+ and LOUT-//ROUT-, but I want to be sure.

    thx

  • SSM3302 POP suppression muting device?

    We have a design using SSM3302 class-D power amp driving a piezo transducer via step-up transformer and matching Ls. The device is configured as a single channel mono amp (MOMO pin 17 pulled up to AVDD) with outputs paralleled. Input is differential AC…

  • RE: Is there an IBIS Model for the SSM3302 ?

    Hello,

    No we do not have IBIS model for SSM3302. The SSM3302 is analog input amplifier and does not have clock and data input/output pins for SI analysis.

    Regards

    Rajeev

  • ssm3302 pop click issue

    Hello,

    I need help with class d amplifier: ssm3302. I've build a prototype board with this amplifier. Every turning off and on ssm3302 using sdnl and sdnr causes a very bad click effect on speakers.

    The audio input is connected with uda1330 dac…