• SSM3302 input pin

    Hi, Support Team

    Regarding SSM3302, I have the following questions, and could you give me some advice?

    When using in Mono mode, is there any recommended process for INR+/INR-, such as Open or GND connection?

    Best Regards,

    NEK

  • SSM3302

    Hi, 

    I've got a question from customer who are trying to connect SE Audio out instead of BTL with SSM3302. 

    I couldn't  find any from Datasheet. Is it ok to use SE instead of BTL to Speaker?

    Thanks in advance,

    Angela

  • SSM3302 gain setting

    Hi 

    I am FAE in Japanese distributor.

    Our customer will use SSM3302.

    The page 18 of datasheet mentions "Gain can be further adjusted to a user-defined setting by inserting series external resistors at the inputs."

    I assume it should be like Figure…

  • About the output of SSM3302

    Hi,

    I have a question about SSM3302.

    The "INPUT CAPACITOR SELECTION" on page 17 of the data sheet states that an input capacitor is required for single-ended use, and it is recognized that single-ended input can also be used.

    Does…
  • SSM3302 output

    Is it possible to wire the outputs of the SSM3302 for a common speaker return?

  • ESD Sensitivity of SSM3302

    Hello,

    Is the ESD Sensitivity of the datasheet defined by the HBM or CDM ?

    Best Regards,

  • SSM3302

    Can be guaranteed 20mA current from VREG output to external circuits?

    Does it depends on PVDD voltage and output currents of the load?

  • SSM3302

    I'd like to use SSM3302 audio amplifier at DC inputs connection, i.e. w/o input capacitors.

    But I can't find data about input and bias currents of its INR/INL pins (via resistors 40 kOhm). Please help.

    Thanks

  • SSM3302 Thermal Exposed Pad connection

    I'd like to separate Power Stage Ground and Analog Ground at a PCB design, and finally both grounds will be connected together aside of the IC.

    To which of the grounds should be connected the Exposed Pad? 

    Thanks,

    Semion

  • RE: SSM3302

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,