• Is available to use SSM2537 for the design of headphones?

    Dear Sir:

    Because we are looking for a ClassD Amp suitable for headphone applications with PDM interface.
    Is available to use SSM2537 for the design of headphones?
    In addition, SSM2537 can drive 32ohm speakers?
    If possible, do you have a [THD + N vs. Output…

  • RE: SSM2537 does not react to pattern control messages

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Is the SSM2537 able to play 6 kHz sampled audio?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Audio processor recommendation for megaphone project

    Michael,

    You may want to look at the SSM4567, SSM2529 or SSM2537.  Note the ADAU1787 can provide I2S output or PDM output to the amplifiers.  The SSM4567 and SSM2529 can accommodate I2S or PDM.  The SSM2537 can only accommodate PDM. 

    In PDM Mode, the SSM4567…

  • RE: Is available to use SSM2518 for the design of headphones?

    Hello Hub,

    The SSM2518 is not designed for Headphone applications. Though it can drive the 32 ohm load if connected as differential load. Please note that the headphone load must be close to the amplifier as the long cables to the load can radiate the…

  • Datasheet of EVAL-SSM2537Z

    Dear Sir/Madam,

    Do you have a datasheet or application note, any document for your EVAL-SSM2537Z?

    I will just buy this SSM2537 and evaluation, study....

    I can confirm EVAL-SSM2537Z page-16 on your datasheet SSM2537' rev.0.

    Thanks, Kaos.

  • RE: 有奖分享——最爱ADI放大器

    SSM2537是一款PDM数字输入D级功率放大器,与现有DAC加D级解决方案相比,具有更加出色的性能。SSM2537是功率敏感应用的理想选择。在功率敏感应用中系统噪声能够破坏发送至放大器的小模拟信号,例如移动电话和便携式多媒体播放器。

    SSM2537采用高效率、低噪声调制方案,无需外部LC输出滤波器。闭环三级调制器设计保留了纯数字放大器的优势,同时又具有极佳的PSRR和音频性能。该调制能够在低功耗情况下继续提供高效率,且PDM输出的SNR为103dB。与其它D类架构相比,采用扩频脉冲密度调制可提供更低的电磁辐射…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…