• SSM2305 input configured in single ended mode.

    We are using SSM2305 in our design. We require clarity about the input capacitor usage in SSM2305.

    Input signal is single ended. 

    The ultrasound signal ranges from 20 HZ to 500Hz, Do we need to have C15 values at the input section as it act as a high pass…

  • RE: Some questions on SSM2305

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Can a SSM2305 be used as a single ended output amplifier with an external LC output filter?

    I'm after a small amplifier to create an adjustable analog voltage with some drive current for a measuring application. If I use and DAC to drive the input then could one of the output pins be used as a pwm version of this signal. Then I'd have a low…

  • SSM2305 input voltage range for SD terminal

    Hi All,

    My customer would like to confirm about the absolute maximum input voltage rating of SD terminal of SSM2305. Is it 0V to +Vdd range?

    Best Regards,

      Ricky

  • SSM2305 Audio Amp Input Range

    Dear Community,

    What is the input range on the SSM2305?  The single supply is 4V.  The signal swings 3Vpp.  I appreciate that this is much larger than the normal "audio" signal.  :-)

    Thanks in advance,

    Kevin

  • Hi is there a pspice model available for the SSM2305 class D amplifier?

    Does anyone have a pspice model for the SSM2305 class D amplifier?

    Thanks

    edward53

  • Reload bitstream in Zc706 on the fly from ARM

    We are developing  a custom design on Zc706 EVM using AD9680.

    I'd like to reload FPGA bitstreams on the fly from the ARM. But when I switch bitstreams the interface to the AD9680 no longer works.

    Inside /sys/bus/platform/drivers

    Xilinx Watchdog                axi…

  • ADAU1761 no sound

    Hi

    I'm using it on my own board with ADAU1761 and MCU (STM32L476) configured as master. The idea is to play and record 22.05kHz audio. I made a simple schematic in SigmaStudio to check if ADAU1761 is working (see image below). Sine tone is generated…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…