• SSM2302: Output overshoot.

    There is about 1.56V overshoot at the output. Is it normal?
    Test condition is in below:  Source is from mp3 played by a computer.   Load
    is speaker, one is 8Ohm, another is 100Ohm. It is connected between the Vout+
    and Vout- in series.…
  • RE: SSM3302

    Hello Chai,

    The problem is that the part is not tested below 7V and it has not been characterized below 7V so there is no guarantee that it will work properly at 5V. There is an internal 5V regulator that will not be regulating but just passing through…

  • RE: HMC625B Reliaiblity

    Hi,

    Here you go. Hope this helps.

    Warm Regards,

    Rachana

     PDF

  • ADI芯片辨识、型号查找

    看看截图: