• Antilog Amplifier with SSM2212

    In the datasheet of the SSM2212 you show a fast logarithmic amplifier using the AD8512 and some specific resistors for temperature compensation (an amazing detail!). For an interface to one of my RF circuits, I need an antilog amplifier. Could you suggest…

  • SSM2212 gain

    The data sheet for the SSM2212 in the 8 pin package says the typical gain is 605 but the 16 pin package says the typical gain is 1800. Is this true? This seems like a huge difference in gain just due to a package difference.

    John S.

  • If MAT02EH is still active

    Analog Device part MAT02EH is still active with same manufacturer part number
    MAT02EH? If the part is not available, Kindly provide us the replacement part
    details.

     

    MAT12 or SSM2212.

  • RE: Log Converter

    FormerMember
    FormerMember

    Houly,

      The SSM2212 and MAT12 are the same die in different packages and different test tapes.

    You can use the SSM2212 spice model which is on the product page.

    http://www.analog.com/en/special-linear-functions/matched-transistors/ssm2212/products…

  • RE: Network Analyzer in Scopy is inaccurate

    Hello Arthur:

    First off just, so you are aware, I'm not one of the Scopy programmers, I wrote the software for the ADALM1000 (ALICE). But I have used / tested M2K / Scopy since development started.

    You make a number of valid points. Here are a few…