• Hiss noise by SSM2166 suppress my audio input

    how we can remove hiss sound from the system?

    I think compressor is capable enough to handle the noise so i don't need external bias circuit then also i had used.

    Kindly review this section and guide us.

  • hissing noise by SSM2166

    Hi,

    I have interfaced SSM2166 circuit with my audio circuit to limit the audio level. When I feed audio input ,output from ssm2166 gives some hiss sound. But without SSM2166 my old circuit has clean audio output and there is no hiss sound. There is no…

  • RE: SSM2166 maximum input voltage

    Hi, Joven

    SSM2166 is internally biased as based on figure 16, and it is expected to be in the level of Vcc/2

    In datasheet says: "A dc voltage of approximately 1.5 V is present at AUDIO +IN (Pin 7)", but this value not equal Vcc/2…

  • Max input level for SSM2166

    Hi, I’m building a bass guitar amplifier and I would like to use a SSM2166 as a limiter just before the class D power amplifier to avoid deep saturation of this stage.

    I’m planning to use a unity gain for the buffer, and a rotation point of 300mVrms…

  • RE: SSM2166 Mute Response Time

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: SSM2166: stereo link, defeat noise gate

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Noise gate setting in SSM2166

    Hello Matt,

    We will not have another good analog solution for you. If you had a microcontroller in the system then you could use the ADAU1761. That part is good in that it has a PGA in the front end and a way to use it as a compressor with some built…

  • Query re setup of  SSM2166

    Hi, I have several datasheets for this device. Revision F removes all setup info. Revision E appears to have the first two steps of set up reversed. I have a revision B from the Web that makes more sense. Essentially the rotation point set up and VCA…

  • RE: i am looking for suitable replacement for SSM2166 (mic preamp)...pls suggest the best solution

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,