• Audio line receiver for new designs

    Hello, 

    I understand that, SSM2141 Differential line receiver is not recommended for the new designs. 

    Hence, please suggest me suitable line receiver for future audio applications.

    Regards

  • RE: Microphone long distance balanced connection

    Hello Roman,

    I am not sure if this is something you want to design and build or purchase already build devices? 

    If you search on the internet for Electret Mic Preamps you will find several kits and designs out there. There are many choices. 

    Then to create…

  • RE: Search for a Differential Line Receiver

    Hi Jino,

          Thank you for your reply!

          Aside from 40 to 100 Vdc input voltage, there is not other special

    requirement. I want to get one Differential Line Receiver with the same

    function and circuit to the SSM2141, which is used to couple a large d…

  • SSM214x Power Supplies

    The SSM2141/2/3 are specified for +/=18V supplies. The SSM2141 and SSM2143 aren't ground referenced so any reason they can't be powered with 24V and GND? The SSM2142 uses GND internally so is it possible to make +V = 24V, -V = 0V, and tie the GROUND…

  • RE: AD8220 driving long cables/capacitances differential

    Hi wildcard96,

    I think the best way to implement your system is to use the last option with some additional. I can say that by using a specialized line drivers and receiver would fit to your requirement. I cannot say that the first two option won't work…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…
  • AD7851 evaluation board

    AD7851 evaluation baord user guide and schematics are no longer on your
    website, can you provide please?

     

    EVAL-AD7851CB user guide with schematic ia attached below.

    Attachments:
  • AD7854 evaluation board

    Could you please provide evaluation board user guide and schematics for the
    AD7854

     

    See attachment

    Attachments:
  • 资源转发---仪表放大器设计指南

    仪表放大器设计指南