• RE: 5532 1st order bandpass for electret mic preamp

    Are you using the SSM2019 microphone preamp (not SSM2219)? That is an audio preamp with the one external resistor gain adjustment, as you've mentioned. On page 6 of the SSM2019 data sheet, there is a table showing the different resistor values and gain…

  • SSM2019 balanced mic preamp - single power supply?

    Can th SSM2019 be run from a single DC power supply, rather than provide a +V and -V?

    I'm planning a balanced microphone amplifier circuit and thinking towards an SSM2019.

    Thanks,

    Eric

  • noise of SSM2019

    Dear Sir/Madam,

    We are using SSM2019 Self-Contained Audio Preamplifier.

    We have observed the noise on our system. Pls refer to the attached file.

    sheet1. Our test circuit diagram.
    sheet2. Waveform which the noise occurred.
    sheet3. Normal waveform…

  • SSM2019使用问题

    SSM2019供电,使用两节相同电池,只是一节11V一节9V,电池串联,+11v接引脚7,-9V接引脚4,0V接引脚5,连接后9v的电池变为固定0.75v,输出也不能正常放大,请问是什么原因呢?

  • SSM2019 fails with high input current

    We are using SSM2019 for balanced MIC pre-amp. It is powered by +/- 15v source.

    Occassionaly a device fails in operation with no apparent reason. When testing failed device with multi-meter it looks like the input stage broke but I can't be sure on that…

  • RE: alternative audio mixer IC for SSM2163

    Hello,

    Unfortunately we don't have a direct replacement for SSM2163,  But in case your interested on other option that uses a discrete solution, you can look at the SSM2019. The part is a self contained pre amplifier with noise level at 950pVrtHz and…

  • RE: Can I use the ADAU1701 as a  balance mic input

    yes, you can use a dedicated mic preamp for this task:

    http://www.analog.com/media/en/technical-documentation/data-sheets/SSM2019.pdf

    This part requires a voltage rail of at least 10 V; +/-5 V or greater. If you do not have that available, your best…

  • RE: Connect microphones to ADAU1979

    what do you mean by 'standard' microphone ?

    if it means dynamic mic, you don't need power to mic

    if anything else, power supply circuit should be designed outside ADC

    with anything, the preamp is needed that amplify audio signal from mic…

  • RE: Poor CMRR Results with AD620

         Byron,

         Where I work we're very happy with the SSM2019 -- although I haven't actually measured its CM response, this mic preamp has proven itself in installations with 200' cable runs.  I do recommend enough input RF filtering to keep out…

  • RE: Designing high gain, low noise, low input amplifier?

    I would suggest an input-amplifier like SSM2019. It can provide the desired gain and includes a differential input. For such a wide range of input signals you may need a option to switch input-gain.

    Although the DSP can provide "digital" gain it may…