• RTI-850 RTI products

    Whether this part obsolete or not? Could you help to give the price if this
    part still in production?

     

    ADI has not manufactured the RTI products for many years.

    ADI transferred the products to another supplier…

    Please have the…
  • AD8138 - Vocm RTI noise

    Question on the AD8138 input referred noise of the Vocm input noise specification:

    The datasheet lists this as 17nV/rtHz, which is more than 3 times that of what the datasheet claims in the features.  Does this noise always apply and scale with BW and…

  • Application returns to wrong place on RTI

    Hi everyone, thanks Craig for help.

    I try to use UART0 interrupts. I initialize EVT8 as isr_uart0_rx, EVT10 as isr_uart0_tx. I use Terminal program to send and receive bytes from PC to my target board. I send one byte to target board, isr_uart0_rx works…

  • RTI error and RTO error and Calculation for error budget

    What is the difference between an RTI error and an RTO error and how do I
    calculate them for my error budget?

     

    The AD8422 is composed of a preamplifier stage that applies differential gain,
    and a subtractor stage that removes the common…
  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • RE: Intermittent Video on ADV7623

    Jarrod,

    To be clear, I'd like to know the value of Cpg1 and Cpg2 as defined in AN-1260.  AN-1260 uses a rule-of-thumb of 5pF each.  I'm looking for a guaranteed specification for these two values.

  • How to modify for compiling in visual dsp 3.5++

    Hi, 

    I am trying to build the old project in visual dsp 3.5++ , which was built in development tool 6.1.  In this project there is .dsp file which as following code

    MODULE/ABS=0 Driver_Runtime_Header;

    .GLOBAL ___lib_prog_term;
    .EXTERN ___lib_setup_everyth…

  • RE: VisualDSP3.5 & 2181 EZKIT

    Hi, thank you for you're answer.

    I have upgraded my software to the October update, wich is working.

    My board come from http://www.kk7p.com/dsp.html , i'm using the windows loader that is on this web page.

    I am finaly able to load a _very_…

  • RE: "Margin for oscillation stop" of the XTAL for decoder devices

    In a previous case a customer had an issue where the crystal would not oscillate at low temperatures. The customer choose the incorrect value for the external capacitors. We have a formula in the "load capacitance" section of apps note AN-1260 that describes…

  • RE: ADV7180 crystal drive level?

    This is also some information in this application note that might be applicable:
    http://www.analog.com/static/imported-files/application_notes/AN-1260.pdf

    -Matt