• rt2378-20

    Greetings all,

    As usual, the data sheet is missing an entire section. It has the timing numbers, but no timing diagram. Does anyone have the timing diagrams for this IC?

    Thanks in advance - JB

  • AD9629BCPZ-20 availibility

    Hi,

    We have a product in now in production, we have difficulties for supplying AD9629BCPZ-20, so we have supplied now AD9629BCPZ-40.

    We are running the sampling rate at 5msps, with the AD9629BCPZ-20 and everything is fine.

    So I wonder if there is any…

  • LT8471: 40V in to +/-20 possible?

    Is it possible for LT8471 to handle 42V input and generate +/-20V bipolar output, 0.3-0.4A per rail? I was looking at figure 10A which is pretty much what I need, but the voltages are a bit off. 

    If it's possible, what should I change besides the feedback…

  • ADV7341 20 bit YCbCr In

    I have an ADV7181 dev board.

    I am checking the ADV7341 on the board for CVBS out.

    I am inserting a 525i YCbCr 10 bit and 20 bit signal into the AD7341, I have disconnected the ADV7181.

    When I set my input for 10 bit it works fine.

    When I set for…

  • AD9840: Operation at 20 MHz

    I have two technical questions to the AD9840AJST (CCD Signal Processor):

    The listed "CCD-MODE SPECIFICATIONS" are they valid in the range of
    20MSPS...40MSPS or where are the MSPS limits for properly results (CCD-Mode
    including…
  • OP777 4 to 20 ma

    Hello every one, i cant resolve this circuit:

    1. i cant get the equation to resolve that.
    2. i dont understand the transistor in the forward loop.

    i need help, any body know how to resolve the circuit.

    Thanks!!

  • HMC624ALP4E operation 20-100MHz

    Dear Sir/Madam,

    I have been using the digital attenuator HMC624LP4E that operates from DC-6GHz, but now I realize that it does not appear at Analog website anymore.

    Instead of this, I have seen the HMC624ALP4E, but it starts from 0.1 to 6GHz.

    Can you…

  • LFCSP 20 - Wrong footprint

  • AD5791 20 BIT DAC

    I downloaded the demo software for AD5791. In a real application can I get better than 5 uV accuracy?

  • 2008-10-02 20:20:29     Open CV compilation problem

    2008-10-02 20:20:29     Open CV compilation problem

    ashwin b (INDIA)

    Message: 63052   

    I am trying to compile OpenCV 1.0.0 for  uClinux R06.

    The configuration command I am using:

    ./configure --build=i686-pc-linux-gnu --host=bfin-uclinux LDFLAGS="-L/home…