• REF198 for supply AD5612

    Dear forum,

    I'm designing a board with one ADC AD7997 and one DAC AD5612. I'm going to use REF198 as a voltage reference for AD7997.

    Could I use the same REF198 to supply the DAC, that use the supply voltage as the reference?

  • REF195, REF198: additional information not in the datasheet?

    Can you please provide the following information for the REF198ESZ ?
    1. Typical Power, (Pd typ)
    2. Maximum Power (Pd max)
    3. Thermal Resistance Junction to Board (Theta JB)

     

    (1) Look at the REF19x data sheet at the “specifications”…
  • 请问REF198能够全年20mA工作保持参考电压输出稳定吗?

    现在准备使用REF198用作产品的基准电压源,想请教这个在全年产品在其20mA输出电流工作过程中能否保持参考电压稳定?具体电压摆幅大吗?

  • the REF IN/REF OUT pin of AD7091r_2 output a voltage which is 6.0V,but the refered voltage is 4.096V provided by REF198 ?

    I am using AD7091r_2,  using REF198 as  thethe refered  voltage,which is   4.096V ,    and  the input voltage of  Vin0  and Vin1  of the AD7091r_2 is from 0 to 6V ,   when the input of Vin0  is 6V  and the input of Vin1 is 0V,  the REF IN/REF OUT pin of AD7091r_2  become…

  • TAGS LISTS: Voltage References

    LT1460
    LTC1258
    LT1021
    LT1027
    LTC1798
    RH1021-10
    RH1021-5
    RH1021-7
    LT6660
    LH0070
    LTC6655
    AD2700
    AD2702
    AD584S
    REF01S
    REF05S
    REF10S
    REF43S
    REF02S
    AD1582
    AD1583
    AD1584
    AD1585
    LT1019
    LT1236
    LTC6652
    REF02…
  • RE: cn-0209

    Hi,

        My maximum input is ±10V.I am planning to take the output from AD8275 to an Arduino Due board(the maximum voltage that its input pins can handle is 3.3V).I am not planning to use AD7193.Sorry Sir,I could not get your point in your previous post…