• Question about REF194

    Hi All,

    REF194 has a current sink spec into the OUTPUT pin?  If it has, what is the maximum sink current?

    Best Regards,

    Kazu

  • RE: AD7920无法读出转换结果

    可以飞线将U6 REF194基准的输出4.5V,引入ADC输入端,再看ADC输出,还跟理论值(0xFFF)相符。

  • RE: cn-0209

    Hi,

    I require an output less than or equal to 3.3V at the output of AD8275.Can I get help regarding the supply voltage and reference voltage that is to be given to AD8275 for this?If I change the reference for AD8275,then I would need to generate this…

  • TAGS LISTS: Voltage References

    LT1460
    LTC1258
    LT1021
    LT1027
    LTC1798
    RH1021-10
    RH1021-5
    RH1021-7
    LT6660
    LH0070
    LTC6655
    AD2700
    AD2702
    AD584S
    REF01S
    REF05S
    REF10S
    REF43S
    REF02S
    AD1582
    AD1583
    AD1584
    AD1585
    LT1019
    LT1236
    LTC6652
    REF02…
  • AD7766-1 @ BF518 SPORT, data integrity issues

    Hello,

    I have some odd behavior of AD7766-1 converter, being read from BF518's SPORT0. Please help me address the problem of the whole system's nonlinearity. Here're the details

    1. I run slow sawtooth as test signal (F=0.01Hz), converter…