• REF191 output pulldown resistors

    Hello there,

    I am currently working on an application where REF191 chip is used. I have a question regarding the output state of the chip when the sleep pin is grounded. The datasheet states the the output is high impedance but it doesnt say how high…

  • REF19x series [REF192, REF191]: allowable sink current at REF192 Output pin

    Hi, i'm Jeong Ho Lee from vpixmedical

    Firstly, i appreciate to your help about last question of potentiometer.

    It really helps!

    Anyway, I have a question about REF19x series.

    We try to use REF19x as a kind of reference(?) voltage at -IN pin of AD8138…

  • AD7091R使用咨询

    使用AD8275和AD7091R-4BCPZ-RL7设计4路ADC采集电路上报给CPLD

    1.在测量0~10V输入时,AD8275的ref1和ref2接GND,AD7091R的ref接2.048V

    2.在测量-12V~+12V输入时,AD8275的ref1和ref2接2.5V,AD7091R的ref接5V(ref191更换为ref195)

    问题:

    1.使用1片ref192是否可以满足4片AD8275的参考电压的电流需求?

    2.AD7091R的muxout直连ADCin在PCB布线上是否有屏蔽要求…

  • AD7091R-4BCPZ设计问题

    使用AD8275AD7091R-4BCPZ-RL7设计4ADC采集电路上报给CPLD

    1.在测量0~10V输入时,AD8275ref1ref2GNDAD7091Rref2.048V

    2.在测量-12V~+12V输入时,AD8275ref1ref22.5VAD7091Rref5Vref191更换为ref195

    问题:

    1.使用1ref192是否可以满足4AD8275的参考电压的电流需求?

    2.AD7091Rmuxout直连ADCinPCB布线上是否有屏蔽要求…

  • TAGS LISTS: Voltage References

    LT1460
    LTC1258
    LT1021
    LT1027
    LTC1798
    RH1021-10
    RH1021-5
    RH1021-7
    LT6660
    LH0070
    LTC6655
    AD2700
    AD2702
    AD584S
    REF01S
    REF05S
    REF10S
    REF43S
    REF02S
    AD1582
    AD1583
    AD1584
    AD1585
    LT1019
    LT1236
    LTC6652
    REF02…
  • 关于ad9244

    有几个关于ad9244的问题想请教

    1. 其数据手册中第6页, Table4中提到 Minimum Conversion Rate 为 500KHz, 同时在第9页对Minimum Conversion Rate 做出了解释:

    我是否可以理解为ad9244的输入时钟应大于500KHz, 否则其性能就会下降?

    为什么时钟低了, 性能就会下降?

    2. 数据手册的第18页, Table9中,  External (外部基准模式) 这一行中有: 1 ≤ VREF ≤ 2.0

        在第21页中又以…