• REF02: TEMP pin

    Hello,

    I have a question about the TEMP pin of REF02.

    The explanation of the TEMP pin has the description in page15 of the REF02 data sheet.

    There is a description that recommends the OpAmp of a low bias like AD8641 to be used for here.

    Is this bias…

  • REF02 action

    Dear Sir/Madam,

    As for your REF02 Vref,

    If REF02 short Vout to GND, then what is the output voltage action?

    1) drop to GND directly soon

    2) when over the some load for a while, and drop to GND

    Otherwise another action?

    Thanks Kaos

  • Temperature Monitor REF02

    REF02 Specifications for Voltage Output at TEMP Pin was changed with Datasheet-Revision J from 550mV to 580mV.

    But all following Revisions (including actual Rev.M) still show the description „…The nominal voltage at the TEMP pin (VTEMP) is approximately…

  • Ref02: Radiation data for lower dosis / values - 5962R8551401VHA

    Is the radiation test report available for the Ref02S - 5962R8551401VHA
    I need to understand how the reference voltage changes with regard to the
    TID(total ionizing dose).
    I mean, the limit values for a total of 100 kRad TID
    are available…
  • TAGS LISTS: Voltage References

    LT1460
    LTC1258
    LT1021
    LT1027
    LTC1798
    RH1021-10
    RH1021-5
    RH1021-7
    LT6660
    LH0070
    LTC6655
    AD2700
    AD2702
    AD584S
    REF01S
    REF05S
    REF10S
    REF43S
    REF02S
    AD1582
    AD1583
    AD1584
    AD1585
    LT1019
    LT1236
    LTC6652
    REF02…
  • RE: AD7685 - 5V Ref and 5V Input, not full scale output?

    Hi,

    Did you follow the AD7685 layout guidelines for your circuit (placing reference decoupling capacitor close to the REF and GND pins, etc)? Please also note that as per the REF02 datasheet, "While the REF01/REF02/REF03 series of references are designed…

  • RE: REF02A Input Voltage from a SMPS

    Hi Brian,

    In general switchers can be noisy, so I'd say filter the output of the switcher to clean it up before bringing it into the REF02.

    I'm going to move this into the Amplifier community in case there is more information from someone there…

  • AD7674基准电压相关问题

    AD7674芯片使用外部基准电压,在ADC工作的时候基准电压对地值会被拉低,ADC不工作的时候恢复正常。ADC摘掉基准电压也恢复正常。

    基准电压芯片位REF02,推测它的带载能力不够,在后面加了电压跟随电路。加入电压跟随电路后,基准电压正常工作,跟随电路输出电压会被拉低。

    请问如何解决?

  • TAGS LIST: Sensors & MEMS

    ADXL78
    ADXL001
    ADXL278
    ADIS16223
    ADIS16240
    ADIS16209
    ADIS16203
    ADIS16201
    ADXL193
    ADISEVAL
    ADXL1005
    ADIS16000
    ADIS16210
    ADIS16227
    ADIS16228
    ADIS16229
    ADIS16305
    ADXL1001
    ADXL1002
    ADXL1004
    ADXL103
    ADXL151
    A…
  • RE: ADC conversion using Instrumentation Amplifier

    Hi,

    What do you think of about my approach basically.

    Alternative 1

    Using 2 power sources +/- 10V and +5V. Feeding Bridge with 10V and op-amps with +/-10V. Using 5 volts to power DAC. Use +/-10V input type ADC.

    Alternative 2

    Using 5V only. Excite…