Hi,
Please give me the resistance values of R5, R6, R20, and VBG Voltage of Figure 33. I would like to calculate the calibration range of trim adjustment circuit which has some difference with figure 35.
Hello all,
I have a noise problem at an oscillator starting at abt 100 kHz up to abt 1 MHz offset from the carrier (see picture).
I measured the spectrum of the power supply - and there is a remarkable noise increase around 500 kHz +/-.Problem located…
Hi,we work on a robotics system with Three 48v Battery pack. I want to design a board in order to switch between three batteries based on the priority.
we need a circuit with a max 40A pike. I found LTC4421 and LTC4418 for this work. As I read in the datasheet…
Hi Zack, upgraded program to 1.0.1.0: now it works!
Hi all, I am doing research for system ID for battery systems and I need to measuring a single cell voltage and set the discharge state of the balancing resistor at rate of less than 1 ms. My current set up is a laptop connected through a serial port…
td is the delay from when clock goes high to when the transition happens on the output. The tMD is the time delay from the falling clock edge to the when the data transitions. tH is the clock high time but that is controlled by your clock source. The…
Hi Ryan,
Please connect to a local ADI FAE.
We are using LTC3566 for a wearable application. We want to use LTC3566 in Type-III compensation for the boost output.
Please share the values for R1, Rfb, C1, R2, C2, R3, C3, Cout, and Lout for 5V/1A output.
The datasheet has the values for 3.3V…