• RE: OP77 offset voltage issues

    This question has been closed by the EZ team and is assumed answered.
  • OP77 Spice model Pin define

    Hi Sir

    Could you please provide OP77 spice model pin define?

    These model have 5 pin

    But I not sure the pin define

    And could you please provide some simulation example about these model?

    Thanks

    Daniel

  • OP77 open loop gain linearity.

    Please expound on the discussion of open-loop gain linearity on page 10 of the OP77 Rev E datasheet.  The write-up does not go into much detail and the plots confuse me.  Both graphs plot some unknown voltage Vy versus the circuit output voltage Vx.  What…

  • 请问OP07、OP77在做单位增益放大器应用时,其电路如何接,有什么建议?

    在OP27的单位增益放大器应用中,贵司的PDF文件中有提示正向端和反向端中间接补偿电容,但是在OP07和OP77的PDF文件中找不到相关的说明,请问OP07、OP77在做单位增益放大器应用时,其电路如何接,有什么建议?

  • RE: OP97 / OP07 spice models

    JW,

    The OP07 is over 35 years old.  The generations have been OP77, 177, 2177, and now ADA4077 and ADA4177.

    For most general work, you could use the OP2177 model.

    Op amp models are macromodels, not primitives, so the model writer can add as much or as…

  • RE: OP177 SPICE model

    Hi harryh,

    thank you for the reaction on my posting.

    The background of my question is: I was trying to figure out differences between the OP77(E) and the OP177, but could not make out anything significant in the datasheets, so I wanted to compare the…

  • OP77AZ/883

    Hello,

    I'm going to use the OP77S, the space qualified version and I also would like to simulate my circuit with spice.

    But on the OP77S product page there is no spice model and on the product page of the OP77 (commercial) there are five model proposed…

  • RE: 请问OP37S和AD574S这两个宇航级型号的结温(Junction Temperature)范围是多少

    经检查,发现几乎所有宇航级的型号,如OP07S、OP27S、OP77S等,在贵司网站上都无法下载其数据手册,共同点是宇航级型号的数据手册的下载网址都是出自“ www.dscc.dla.mil”(如OP07S的数据手册网址为http://www.dscc.dla.mil/Downloads/MilSpec/Smd/98639.pdf),而这个网站在国内是打不开的,请问是否有解决这个问题的方法?否则宇航级型号的数据手册无法在贵司官网中下载和查看。我如果想查看这些数据手册的话,该向谁要?

  • RE: AD630 Output Noise Source

    Nick,

      It's a complicated issue.  Let's do a thought experiment.  

    Case one is a part that has ten customers, each one buys $100k/year.  So one customer redesigns his

    product and stops buying.  Any semi company would keep making the part.

    Case two…

  • RE: short pulse amplifier

    what is Y1 in your schematic. I do not follow exactly what you are doing but you can look at figure 36 of OP77 datasheet hwich gives you detection and amplification. You may need to do adjustment for your needs.

    http://www.analog.com/en/all-operational…