• U3-E and U4-E in ADuC SAR Eval Schematic ?

    The ADuC SAR Eval Schematic (https://www.analog.com/media/en/technical-documentation/evaluation-documentation/151851ADuC_SAR_PCB_A3.pdf) lower left corner shows a combination of 2 OP491 stages labeled U3-E and U4-E.  Furthermore there's a label "V0 = 2V1…

  • AD8515 Wein Bridge Oscillator LTSPICE design fails

     PDF PDF PDF PDF

    I am trying to use LTSPICE to simulate FIgure 38 of AD8515 Rev E Datasheet, "Low Power Wein Bridge Oscillator". 

    I downloaded and imported into LTSPICE XVII the spice subckt for AD8515, and wired up the circuit and got "flat line…

  • OP293: Available as bare die

    I require an op-amp with a fairly basic electrical spec but it must be
    available in die form for incorporation onto a microwave substrate in a sealed
    module.  It must operate from a single +5v supply and the input voltage range
    should extend down…

  • ADUC841输入的时候究竟需不需要加电压跟随器做缓冲???

    这是第二个我用的ADUC8XX的案子了。对于我要问的问题,我就简单明了说吧。

    第一、我用的是ADUC841

    第二、我现在用的是ADC0通道,输入的电压源是1.5V

    第三、我用的是内置基准源。

    第四、我用的WASP测试的,用这个排除程序问题。

    我的问题是,1.5V在2.5V基准下应该是0x0999   ...现在就只有0x0773左右?(1.2V)

    之前用的那个ADUC814的解决办法是接OP491解决的(ADI开发板给出的方案)

    我也知道,加上去肯定就没问题了。

    我想问的是这个东西不加外部缓冲如何采集到正确的电压值…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • 问题: [征文]关于ADUC814线性度的几点问题【问题解决】

    为了更好的说明问题,下面摘取了21组采集电压对比

     

    实际电压 被测电压 偏差
    2985 2990 -5
    2925 2931 -6
    2836 2842 -6
    2738 2731 7
    2656 2664
  • ADI运算放大器选型指南

    ADI运算放大器选型指南

  • operational amplifier without internal bias-compensation

    Do you have amplifier (opamps) without internal bias-compensation?

     

    We have two different types of bipolar amplifiers in our portfolio. Simple
    bipolar and bias-compensated bipolar amplifiers.
    (See app_eng.pdf on page 9 bottom left)

    Opamps without…