Hi
1- Is it possible to use op467 with single supply with "5 v, 9 v, 12v" ? datasheet has only dual supply example.
2- I would like to use op467 for band pass filtering between 20Hz to 500 khz is it possible ? How should i do it ?
I look forward…
Hi
1- Is it possible to use op467 with single supply with "5 v, 9 v, 12v" ? datasheet has only dual supply example.
2- I would like to use op467 for band pass filtering between 20Hz to 500 khz is it possible ? How should i do it ?
I look forward…
用OP467做电压跟随器,输入正弦信号为200KHZ,峰峰值才0.6V,为什么输出波形会失真为三角波?OP467的压摆率170V/μs,应该不是因为压摆率不够导致的吧。
Hello,
I am trying to build an amplifier for quite a wide range of frequencies (40Hz - 200 kHz). I wanted to use OP467 since it has quite a wide bandwidth. So, using one section of OP467, I built an inverting amplifier with a gain of 10. However, I am…
Hi,
The data sheet for the OP467 & OP467S lists the power supply current as 12mA with +/-5V supplies.
Is this per amplifier our for all 4 amplifiers (entire chip)?
Our measurements would correspond with this being for all 4 amplifiers (the entire…
Hi, I need the Junction-to-board thermal resistance of the OP467S CERDIP-14. This information is not on the datasheet.
I have download the PSpice model for OP467. But when I started to use it, its pins name are 1, 2, 99, 50, 27. What' s the meaning of these numbers? Which one is -IN (or +IN, V+, V-, OUT) as described in the PDF?
When I used the pspice model of OP467, I found its pin name are 1, 2, 99, 50, 27. What is the meaning of these numbers? Which one is +IN (or -IN, OUT, V+, V-) as described in the datasheet?
Hi Jun667,
What sampling rate are you working with for the ADC, and what is the udpate rate for the DAC?
The OP467 is much faster than the OP471. The best choice of amplifier would still depend on the requirements of your application. If you can provide…
Hi Mickael,
You can view our quality website @ Analog Devices' Quality & Reliability Program | Analog Devices.
Specific product reliability data can be found @ Wafer Fabrication Data | Analog Devices. Enter the OP467 part number to view details…