• [OP400S] Question

    Hi

    Im daejin in working SATREC INITIATIVE

    Are these devices use the same raw material set(ex, die) and are processed on the same Class S certified assemble and test line?

    5962R8777102VCA (OP400AY/QMLR)

    5962-8777102VCA (OP400AY/QMLV)

    If there are the…

  • Op400 issues

    My question is as below,

    are these devices use the same raw material set(ex, die) and are processed on the same Class S certified assemble and test line?

    - 5962R8777102VCA (OP400AY/QMLR)

    - 5962-8777102VCA (OP400AY/QMLV)

  • op400 issue

    Hello

    are those parts use die? Just applied different quality level(test)?

    5962R8777102VCA (OP400AY/QMLR)

    5962-8777102VCA (OP400AY/QMLV)

  • OP400 max input current

    Hello,

    I am looking for the maximum input current for the OP400. Thanks

    Josh

  • OP400 Max Input Voltage

    I'm using the OP400 amplifier in what is basically a classic non-inverting buffer application.

    The positive input is subject to large voltage transients where I have 1N5806 diodes connected between the input and positive/negative supply rails of…

  • OP400S: no power up sequence required

    Do you need a power sequences to power up the OP400S?

     

    We do not have any information on power up sequence, but it doesn’t hurt to
    practice bringing up the negative supply first.
  • RE: Can ADA4000-4 work on +-18V power supply?

    Hi, Anna.

    Thank you for your reply! Yes I need quad opamp. OP400 may be a choice.

    Best regards,

    Billy

  • RE: Spice Model for OP-400A

    mk,

      Some spice models do no model current draw correctly.  If this is not one of your critical parameters, I would ignore.

    Also, the OP400 is a very ooooooold part;  I would look at ADA4622-4.

    Depending on critical your signal path is, I would also use…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • RF/High Speed Signal Prototyping

    I'm trying to use the AD600 (as well as some other components, but the AD600 for now) in a a high speed application, but do not have circuit boards yet.  The part does not have an evaluation board, but I'm not sure if I can use the white/breadboard…