FAQ
Hi,
We met some issue on our product with OP2177 device.
With a date code OP2177 A#830 5002 ==> our product works without problems.
With a date code OP2177 A#932 6453 ==> our product doesn't work.
Could you communicate if the PCN#18_0060 is applied…
Hi. In our application, the OP2177 output is disconnected for a period of time, and the feedback loop is broken resulting in the OP2177 output going to one rail or another (+ or - 15 V). We then close the output relay and the feedback loop is closed again…
Hi Areski,
My initial assumption was that this amplifier belongs to the OP07 family. And we should expect similar input protection circuitry. But you can't say anything unambiguous, because there is no uniformity in the data sheets. I believe that OPX177…
Hi Team;
OP2177 at +/ -15v power supply, the input voltage range is +/ -13.5v.
Is there any device with similar parameter, but is rail-rail input/output at +/ -15V?
many thanks;
Bell