• OP177 SPICE model

    I have downloaded the SPICE model file for the OP177 but found that it actually contains the model for the OP1177.

    Where can I get the proper SPICE model file for the OP177 ?

  • RE: OP177 power sequence

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Offset Voltage adjustment for OP177

    Dear Sir/Madam,

    Our customer asked th following question to me.

    As for your OPAMP OP177GSZ,

    your datasheet shows the adjustable offset voltage adjustment range is +/-3mV typ by adding 20kohm POT on Rp.

    So if we need it +/-6mV, then what is the external…

  • 442 - I cannot find the datasheet for the 442 (old OPAMP Module)

    I cannot find the datasheet for the 442 (old OPAMP Module)

     

    Please find attached.

    A suitable replacement is the OP177 or OP1177.
    Attachments:
  • RE: OP-177

    The OP177 is not RR output.

    You need a cap on the LM317 adj pin to ground.

    What is the diode doing on the output of the op amp??

    Harry

  • RE: OP177G / Difference Amp

    Dear Harry,

    Thanks for the informative reply. I have hit the books since your reply and made an excel sheet that incorporates all the details (input offset volts, current, input bias current, Rth of the wheatstone bridge). Waiting to get back to office…

  • AD620, digitally adjusted reference pin

    Hi,

    I use AD620 in order to amplify my loadcell signal. I have +/-15V present. I regulate these voltages to 10V and -11V. I use 10V to excite loadcell. Also I use 10V to power AD620 and OP177 op-amps. (There is a filtering circuit after AD620 with couple…

  • RE: OP07 SPICE Model

    Mr. K,

    The OP07 was a first generation precision op amp.  I would not do a new design with it.

    We have done several generations since then:  OP07 -> OP77 - OP177 -> OP1177 -> AD8675/AD8677.

    The newer parts have spice models which can be found…

  • RE: AD620 drift

    dclm,

      20V / 65536 =  305 MICROVolts??  Not millivolts??  Do you mean microvolts all the way though your reply?

    Is this measured at the output of the AD620 or the second OP177??

    Is your "16bit A/D module" a monolithic IC or truly a module?? 

  • RE: short pulse amplifier

    what is Y1 in your schematic. I do not follow exactly what you are doing but you can look at figure 36 of OP77 datasheet hwich gives you detection and amplification. You may need to do adjustment for your needs.

    http://www.analog.com/en/all-operational…