• Is there something wrong with the OP162 spice model?

    I'm simulating a 4 stage filter/amp circuit using the OP162 within Altium and Multisim. I'm getting very strange outputs compared to using other TI branded opamp. When I try to simply create a voltage follower using the OP162 with an input of 100uV sin…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • RE: 非常实用、超详细的锁相环常见问题解答~

    问题:参考晶振有哪些要求?我该如何选择参考源?

    答案:波形:可以使正弦波,也可以为方波。

    功率:满足参考输入灵敏度的要求。

    稳定性:通常用TCXO,稳定性要求< 2 ppm。这里给出几种参考的稳定性指标和相位噪声指标。

    名称 频率范围(MHz) 频率稳定度(ppm) 相位噪声dBc/Hz@10kHz 价格
    普通晶体振荡器SPXO 1~100 +/-10~+/…
  • RE: HMC767 reference divider, lock detect

    Hi, 

    Let's work through each issue and see if we can get it to lock.

    1) I suspect that the reason the part rails when you change the R divider value is that you aren't "re-training" the LD window. Each time the R divider is changed you need to tog…