• VTTI and VTTO supplies to input and output pin association

    By chance, are VTTIW pins 9 and 18 associated with (IP0/IN0, IP1/IN1, IP2/IN2) and (IP3/IN3, IP4/IN4, IP5/IN5), respectively? Can VITTW pins 9 and 18 have different voltages? Same question for VTTIE relative to pins 55 and 64 association with (IP6/IN6…

  • ADN4612 Design Support Files

    Attached and linked are files supporting the development of systems using the ADN4612, 11.3Gbps 12x12 Digital Crosspoint Switch.

    We recommend that, if you download and use this document, you subscribe to email notifications for either the entire forum…

  • ADN4605 Design Support Files

    Attached and linked are files supporting the development of systems using the ADN4605, 4.25Gbps 40x40 Digital Crosspoint Switch.

    We recommend that, if you download and use this document, you subscribe to email notifications for either the entire forum…

  • ADN4604常稳工作问题

    我们设备的应用情况如附件图中,一路DVI信号进来后分两路出去。一路给后端进行采集,一路直接到DVI接口进行显示。问题:在常稳拷机的情况下,大概在24-48小时之间ADN4604的输出两路信号消失,即DVI接口接入显示器看不到图像,后端也采集不到信号。

       2、我看了EVM设计,有一个地方我存在异义。ADN4604的VEE信号,EVM图示中是

    ,我设计中是直接接GND。这个地方是否会有影响。

  • ADN4605 channel status registers

    I am able to access ADN4605 device and can access all the registers. But all the channel registers are showing 0x3F. I did not understand this issue? Is it software or Hardware issue?

    i2c write at address 0x0 data 0x1

    i2c write at address 0x0 data …