• MAT14 - wrong figure 5 in Datasheet  Rev A 10_2012

    My customer has problems with Figure 5 of the MAT14.  Of the datasheet.
    (Base Emiter Volage versus Collector Current)

    The MAT 14 shows a change in the slop at about 500uA
    while the MAT04 did not have a change in the slope

     

    The graph in the datasheet…

  • MAT14 - Specification at high collector current, Maximum collector current

    Hello,

    The MAT14 data sheet, Rev A 2010 specifies absolute maximum collector and emitter current as 30mA. 

    Does this specification  restrict current for each of the four transistors individually, or does it restrict aggregate current for all four transistors…

  • MAT14 Cebo spefification

    Hi All,

    I received question mail from my customer as next.

    The data sheet of MAT14 says that Cebo: 40pF typ at Vcb=15V, Ie=0, and f=1MHz.

    My understanding of the Cebo is base-emitter capacitance at collector is open.

    If my understanding is correct…

  • RE: MAT14 vs. MAT04

    Hi, Ricky.

    According to the product owner, the figures in the datasheet of MAT14 are incorrect. They gathered new data, shown below, and will update the datasheet.

    Regards,

    Anna

  • RE: 请问MAT14ARZ耗散功率是多少?

    Hi Emma,

    您下面这个问题,之前有问过ADI的技术,回复如下:

    “这个要看客户用在什么样的电路结构下。

    比如手册图18的配置,功耗就是4倍的IOUT乘以MAT14中1,3点之间的压差。

    数据手册第8页的图18。

    http://www.mouser.com/ds/2/609/MAT14-879573.pdf

    希望以上信息能帮到您。

    Best Regards,

    Jun Liu     (刘 珺)

    Mouser Electronics Shanghai – Line Card<…