• About the LTP5901-IPM Performance Testing

    How far is the maximum access distance between two LTP5901-IPM devices?

    When using the device LTP5901-IPM networking, what is the delay between the two devices?

  • LTP5902-WHM gets prolonged "Not ready to send" alarm while in OPERATIONAL state

    I am running an LTP5902-WHM in an office which has several other similar devices, all talking to an Emerson 1420 WHART gateway.  The Emerson is about 30 feet from my LTP5902.

    My LTP5902 is in an OPERATIONAL state, sending data to the gateway using "Send…

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A
  • RE: About Implementing Wireless BMS - With LTC6810 and SmartMesh IP.

    To integrate LTC6810 with LTP6901-IPM you need to connect both of them via SPI. 

    I can see LTP5901-IPM has a SPI port( pin 38,39,40,41)  which can be used to connect to SPI of LTC6810. 

  • RE: The Voyager kit operates wirelessly, what wireless technology is used?

    The Voyager mote includes Analog Devices SmartMESH wireless technology. A robust low power SmartMESH LTP5901 board is included with chip antenna.

    The Voyager kit also includes a SmartMESH IP manager, which is used as a USB dongle in your PC and serves…

  • Wireless Current Sense

    Continuing with our series, Combo Circuits from the Lab, join Kris Lokere as he tells us what exactly makes Wireless Current Sense.

    Measuring the current that flows through a sense resistor seems easy. Amplify the voltage, read it with an ADC, and…

  • 工程师博客分享——从信号链、电源管理到无线组网,真正的无线电流检测电路是这样的

    上期的参考电路,大家表示很感兴趣→——采用ADI/LTC产品组合的超高精度可编程电压源

    那就继续我们的“组合参考电路”系列,今天的电路将告诉我们如何进行无线电流检测。

    测量流经检测电阻的电流似乎很简单。放大电压,用ADC读取,不就知道电流是多少吗;但如果检测电阻本身的电压与系统地电压相差很远,检测就会变得比较困难。典型解决方案是在模拟域或数字域消弭该电压差。但这里介绍一种不同的方法——无线。

    模拟电流检测IC是紧凑型解决方案,但其可承受的电压差受限于半导体工艺。很难找到额定电压超过100V的器件…

  • 荣获“年度最佳物联网产品 Ace 奖”的SmartMesh IP™ 网络,你真的了解吗?

    SmartMesh IPTm 网络荣获“2017 年度最佳物联网产品”Ace 奖,该奖项授予有助于进一步实现物联网的新技术、服务或最终应用。

    SmartMesh IP 嵌入式无线网状网络可在恶劣的工业环境中实现 > 99.999% 的数据可靠性和超低功耗。”就这一句话,足以知道SmartMesh IP 的厉害了吧哈哈哈

    SmartMesh IP 网络由高度可扩展的自成形多跃点无线节点网格和网络管理器构成,无线节点称为智能微尘,用于收集和中继数据,网络管理器用于监控和管理网络性能和安全…