• Why use randomization?

    Dear all,

    I seem to have some trouble understanding the benefits of output randomization, in my case using the LTM9009-14 series. I have to mention that I use it for sampling "slow" waveforms, and am not familiar with SDR applications, SINAD, SFDR, and…

  • 2011-01-10 14:14:47     workqueue

    2011-01-10 14:14:47     workqueue

    Chris Brissette (UNITED STATES)

    Message: 97302   

    I have been hunting a random lockup, happens about once a week. Seems like it has something to do with the using the ttybf1 uart.  I have been looking to where workqueue…

  • [LTM9006-14]

    The Vcm on My Demo board DC1751 doesn't have output,is it wrong?And what the output type of FR and DCO ?LVDS?

  • RE: ADF4356 for ADMV1013/14

    Hi,

    The ADMV1013 should still work (i.e there will be conversion gain) but at a decreased level along with decreased linearity (OP1dB and OIP3). At 25C there will be only a small difference in conversion gain. These effects will be more pronounced at…

  • RE: LTC2153-14 CLKOUT

    The CLKOUT will follow the ENC signal with a small delay.  If ENC is high then CLKOUT will be high shortly after that. 

    The default it 0 degree phase shift

    There is no reason to dynamically change the phase of the output clock.  It is something you set…

  • RE: LTC2314-14 not working

    NCS should not go high and then low in between the two groups of 8 SCK pulses.

    Please provide a waveform for SDO.

    There is 1 cycle of latency on this part, so the first conversion result will always be garbage. If multiple conversions are done, do all…

  • LTC2258-14 No output or CLKOUT

    We are trying to use the ltc2258-14 with the serial programming mode, Double data rate CMOS.  We can not get any output on the clkout line or any of the data lines.  We have also been unable to read any of the mode registers.

    Any thoughts as to why we wouldn…

  • RE: 14-bit DTS

    This question has been closed by the EZ team and is assumed answered.
  • LTC2256-14 hold time

    Hi,

    Could You please clear some things for me:

    The datasheet for the device stated that the conversion starts at the rising edge of ENC+ signal.

    Is the sample-hold internal capacitor fed with input signal during whole high time of ENC signal or for some…

  • RE: Tcyc of LTC2310-14

    Tcyc max is a carryover from ADCs that use the SCK to perform the conversion. If 1/Fsck was too long, the hold capacitor would start to lose charge through leakage and the conversion result would lose accuracy. The LTC2310-14 has an internal clock to…