• Does LTM9007-14 ADC output data in MSB first format or LSB?

    Hi, 

    I'm currently working with an LTM9007-14 ADC and I wanted to confirm if this ADC outputs the data serially MSB first on the rising/falling edge of the data bit clock?

    regards, 

    Luis

  • Single Ended - Differential conversion phase shift issue

    Hi,

    I am trying to drive 14 bit ADC( LTM9007-14) using two op-amps.( What I do is converting single ended signal to differential signal) I have two different configurations that seem to work for me. But when I run a simulation in LT Spice I see slight…

  • 2011-01-10 14:14:47     workqueue

    2011-01-10 14:14:47     workqueue

    Chris Brissette (UNITED STATES)

    Message: 97302   

    I have been hunting a random lockup, happens about once a week. Seems like it has something to do with the using the ttybf1 uart.  I have been looking to where workqueue…

  • [LTM9006-14]

    The Vcm on My Demo board DC1751 doesn't have output,is it wrong?And what the output type of FR and DCO ?LVDS?

  • RE: ADF4356 for ADMV1013/14

    Hi,

    The ADMV1013 should still work (i.e there will be conversion gain) but at a decreased level along with decreased linearity (OP1dB and OIP3). At 25C there will be only a small difference in conversion gain. These effects will be more pronounced at…

  • RE: LTC2153-14 CLKOUT

    The CLKOUT will follow the ENC signal with a small delay.  If ENC is high then CLKOUT will be high shortly after that. 

    The default it 0 degree phase shift

    There is no reason to dynamically change the phase of the output clock.  It is something you set…

  • RE: LTC2314-14 not working

    Please provide oscilloscope waveforms showing CS, SCK and SDO and a schematic.

  • RE: LTC3779 Schematic for review

    I hope you will get more idea of the requirement from the below table, Input is from an alternator with variable magnitude and frequency. System design is in such a way that, at low speed (low input voltages), load demand is less.

    Input

    Freq

    Vin

  • RE: 14-bit DTS

    This question has been closed by the EZ team and is assumed answered.
  • LTC2258-14 No output or CLKOUT

    We are trying to use the ltc2258-14 with the serial programming mode, Double data rate CMOS.  We can not get any output on the clkout line or any of the data lines.  We have also been unable to read any of the mode registers.

    Any thoughts as to why we wouldn…