The Vcm on My Demo board DC1751 doesn't have output,is it wrong?And what the output type of FR and DCO ?LVDS?
I was wondering if I can drive input pins of LTM9006-14 with single ended DC voltage? Datasheet says "Theanalog inputs should be driven differentially". Can I just ground AIN1- pin and provide dc voltage to AN1+ ?
DC1751这块Demo接上电之后Vcm是不是应该有输出,我的Vcm没有输出,不知道为什么?还有LTM9006的FR和DCO也是LVDS输出吗,还是什么输出?
我现在在用LTM9006的一款DemoDC1751,但是它的接口不利于我的信号的接入,所以我想换成另外一款同样芯片的DC1884的Demo,不知道可不可以。这两款接口如图所示
2011-01-10 14:14:47 workqueue
Chris Brissette (UNITED STATES)
Message: 97302
I have been hunting a random lockup, happens about once a week. Seems like it has something to do with the using the ttybf1 uart. I have been looking to where workqueue…
2011-09-14 14:43:03 user spi
Dario Bueno-Baques (MEXICO)
Message: 103388
Hi everybody:
I planning to develop an application for the bf537 stamp where is necessary to acquire some data from and ADC (16 bits simultaneous sample i.e like AD7655) make…
2008-05-14 14:34:13 Memory Protection
Henning Manteuffel (GERMANY)
Message: 55833
I connected an FPGA to the Blackfin address/data bus for accelerating arithmetic computations.
Is there a way to unprotect certain addresses in user space so that…
2008-01-14 14:07:12 ~~Many Thanks~~
Kris Dickie (CANADA)
Message: 49562 I think it's important to give the BF-uClinux support team credit. I run a support forum for my company as well (although much less traffic), and I know how demanding it can become…
2011-03-14 14:18:22 Problem with CONFIG_DEBUG_EARLY_SERIAL
Timur Aydin (TURKEY)
Message: 98924
I was debugging an intermittent boot issue with my blackfin BF537-0.3 board. I defined the CONFIG_DEBUG_EARLY_SERIAL option in the hope of getting more…
2010-11-14 01:14:10 EZ-Kit for BF533
Jawad Riaz (PAKISTAN)
Message: 95825
Hi..
I am trying to install linux on a EZ kIt for Blackfin....I have configured the host PC with linux GCC and other repositories...I need help on how to configure the toolchain…