• RUN Pin Threshold on LTM8078

    Hi,

    The datasheet of the LTM8078 gives only a single Number for the threshold-voltage of the RUN-Pin (0.74V)

    But whats about the tolerances of this value? There sure is some hysteresis...?  

    Thanks. 

  • LTM8078 LTPowerCAD

    Hi,

    when will the LTM8078 be availiable in LTPowerCAD?

    Regards

    Andreas

  • LTM8078 TRSS1 TRSS2 pins

    Hello,

    I'm going to use LTM878 in my design . Starting from a nominal 24V I would like to generate

    - one 3.3V 2A using one LTM8078 (U1)  configured with shared loads and TRSS1 and TRSS2 pins shorted together as suggested in datasheet

    - one 1.8V (0…

  • RE: LTM8078 OUTPUT OSCILLATED

    Hi Anglic,

    During testing/trouble shooting, you may also short input and/or output inductors/FBs, to see if the issue will be improved/solved.

    Thanks.

  • LTM8078 Feedback Resistor Equation

    Hi, I would like to use the LTM8078 uModule regulator but am unable to find the resistor feedback equation to generate the correct output voltage for a given resistance. 

    Also, is there a Spice model for this device? 

    Many thanks! 

  • Positive to negative -4V converter via LTM8078

    Dear Sir or Madam 

    I'm gonna  to apply LTM8078 to generate a -4V power supply  .

    where ,VIN = 15V ,Vout = -4V ,Fsw = 1.4MHz, spread spectrum modulation .

    here is the schematic , Please help me have a check , Will it work well in excellent performance…

  • RE: Design Parameters for LT3506

    Hello,

    in your scenario I would use a different for two reasons:
    1. We have synchronous (more efficient+space saving) dual buck regulators in our portfolio.

    2. More than that the LT3506 won't work under all conditions, as he needs more Vin to start than…

  • ADI 全新中文资料(2020 年 4 月)