• +/- rail from LTM8068

    I would like to use the LTM8068 to drive various opamps. I like the galvanic isolation and the noise is acceptable. 

    As I require a +15V / -15V rails, I intend to use two LTM8068. (Vout2+ is tied to Vout1- for the center tap)

    My question: The inbuild post…

  • LTM8068 spice model

    How do we set the Vout1 voltage on the LTM8068 spice model? The spice model does not have the FB1 pin.

  • Parallel driving LTM8068

    I'd like to drive redundantly by the following composition.
    (A fellow operates as the insurance when breaking.)

    Would there be a problem with this how to use?

  • -ve voltage Rail using LTM8068

    Hello,

    I would like to use LTM8068 for generating -15V. For this, I connected Vout1 to GND. VOUTN and VOUT2 are connected together and output is taken from VOUT2, VOUTN. I am attaching the schematic. Please let me know if the attached design is proper…

  • CMTI data for LTM8067/ LTM8068

    Hi! I am looking to use LTM8067/ LTM8068 to power gate drivers. Can you provide some data on common-mode transient immunity (CMTI) for these micro-module DC-DCs. Thanks.

  • DC DC Converters


    I would like to configure LTM8068 for a regulated output of 15 V. I understand that the input voltage span for this configuration is 2.8V to 29V. But as per my requirements I need an input span from 16-36 V DC. Can i extend the max voltage to 36V?

    If not…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032