• LTM8065 - small capacitor between Vout and FB pin

    Hello,
    I would like to ask what is the function of the small capacitor between Vout and FB used in the LTM8065 component.
    Thanks
  • LTM8065 parallel output

    Hello

    It's possible to parallel the outputs of two or more LTM8065 to obtain more current?

    Thank you

    Gianluca

  • LTM8065 Cout selection

    I will use the LTM8065 for two applications: 5V and 7.5V outputs.  Table 1 lists Cout=22uF 6.3V 0805 for a 5V output.  The LTM8065 eval board uses 47uF 10V 0805 in parallel with 10uF 25V 0603.  Why the difference from table 1 to the evaluation board for…

  • About LTspice model of LTM8065.

    Hi all,

    I have a question about the LTspice model of LTM8065.
    Does this Spice model consider iron loss?

    If you have a question, please let me know.

    Best regards,

  • RE: LTM8065 how to select optional SBD and bulk cap

    Dear tkozono,

    Thank you very much for your support.

    I've additional questions by the customer.  Could you please let me know ?

    Q1. If a sudden voltage change occurs during hot swapping, does the soft start function not work ?

    Q2. Should the soft start…

  • LTM8065 VOUT CALIBRATION

    I'm trying to fine tuning "vout" of ltm8065 by changing the value of Rfb.
    Is this the right approach?
    Thanks


    
     

     

  • RE: LTM8065: Is it safe to use the +12Vin specs for a  +4.5 - +5.5Vin design?

    Hi dagr,

    The 5Vout configuration lists an input voltage range from 6.5V to 40V because the LTM8065 is a step-down uModule.  This means it can only make an output voltage lower than the input voltage.  The LTM8065 will not be able to output 5V with 4…

  • LTM8064 OUTPUT capacitor

    I will use LTM8064 at 19V,12V,9V.


    By datasheet ,LTM8065's Cout is used Tantalum capacitor.

    I want to know why LTM8064 use Tantalum .

    For example " need low ESR." or "need large capacity."

    if we can it ,we want to change Cout from…

  • LTM4622 Negative Output

    Is it possible for LTM4622 to generate negative output? Just like the one described in LTM8025 or LTM8065 datasheets (attached)?

    Thank you.

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032