• 关于芯片 LTM8064的一些咨询。

    此芯片能否反向使用?即当VIN 不加电压,VOUT加5V电时,VIN能否稳定输出电压?谢谢!

  • 关于LTM8064双象限运行的一些咨询。

    看datasheet上说这个器件可以双象限运行。

    若输入端无电压,输出端的电能能否传到输入端使用?

    另,贵公司还有什么双向DC-DC模块?

  • LTC3649 how do i control the current overshoot when using current limit featuresame problem with LTM8064

    LTC3649 how do i control the current overshoot when using current limit featuresame problem with LTM8064

  • LTM8064能否当双向DCDC变换器使用?贵公司有双向DCDC模块?

    我的需求是:母线经BUCK给电池充电,电池也能给母线供电使用。  贵公司有没有合适的双向DCDC模块?40V-30V左右即可。

  • LTM8064 shows small output voltage error (voltage drop) under load.  What is the normal drop?  Programmed Vout = 29.5V, but with 3.5A load it drops to ~28.5V

    I have 3 of them in a load sharing circuit.  Under modest loads, everything it OK, but when I increase the load to ~3.5 - 4 A, there is a slight (~3%) drop in output voltage.  That seems a little high for a feedback regulated supply.  Sharing of load is…

  • RE: Performance of LTC3588

    Hi explorer_1,

    Apologies for the delay. Based on my understanding of the LTC3588, the harvested energy is stored in the input capacitor connected on the CAP pin, not on the output. If you need a supercapacitor charger, you may take a look at these products…

  • Questions about the current consumption of the LTM8054 at no load

    Hi,

    I have a few questions about the LTM8054.

    In the LTM8054, a current consumption of about 200mA flowed despite no load.
    There was also a slight device heat generation.
    This occurred in the circuit diagram described in data sheet P23.
    As a countermeasure…
  • RE: Part validity & Datasheet

    Hi,

    I don't see this part in datasheet or in website so it means not available for purchase. You may contact local ADI sales to inquire further.

    You can refer to the valid part numbers at the product page in link below. Also the datasheet for product…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032