• LTM8052 output energy recuperation

    Hi support team,

    Suppose the input voltage is 28V, the output voltage is 18V, and there is a large (500 uF) capacitor at the output. Now, the output voltage is made to decrease to 12V by controlling the feedback. The questions are:

    1. What is the discharge…

  • LTM8052 sink mode

    Hello support team,

    I'm using an LTM8052 (to be sure, without "A") module in a prototype power supply. The current limits are set to maximum (both CTL_I and CTL_T tied to VREF).

    The design includes 200 uF input capacitance and 500 uF output…

  • LTM8052 shutdown output high impedance?

    I would like to know when LTM8052 module is shutdown, what is the mode of Vout pins. Are they in high impedance mode? If there is a external voltage there, will there be any leakage current from LTM Vout pins. If any,  how much will that be? Thanks. 

  • LTM8052 soft start time

    Hello support team,

    what is the soft start time of the LTM8052 power module? The datasheet says the charging current of the soft-start capacitor is 11 uA, and that the output voltage ramps during soft start, but it is unclear what is the voltage across…

  • LTM8052 LGA and BGA package

    Hi 

    In our design, we are using LTM8052AEV. But we don't have enough in stock. 

    In the meanwhile, we have a lot of stock of LTM8052AEY. My question is, can we use  LTM8052AEY on board which we designed for LTM8052AEV without any negative impact?

    Looking forward…

  • LT3128 in cascade configuration

    Hello, 

    Is the LT3128 capable of being set in cascade like the LTM8052 for chargin/balancing a set of 6 supercapacitors (from the same power source of 5V)?

    That would be 3 LT3128 charging 2 supercaps each, but having the all 6 in series at the same time…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032