What is the definition of "efficiency" used in the corresponding data-sheet of LTM8048?
I would expect that: efficiency = total output power / total input power.
Is this assumption correct?
Reason for this question: separate plots which indicate…
What is the definition of "efficiency" used in the corresponding data-sheet of LTM8048?
I would expect that: efficiency = total output power / total input power.
Is this assumption correct?
Reason for this question: separate plots which indicate…
Hi
I wanted to use LTM8048 part for our high speed signal isolation project. Ordered bunch of LTM8048EY#PBF and one DC1560A. Firstly, I configured two output of EVAL board to 3.3V and 5V output according to datasheet. Connected some very light load and…
I would like to use an LTM8048 (actually, two of them in series) as a power supply for an isolated gate driver. I didn't find any data on the datasheet regarding input-output parasitic capacitance or CMTI.
Do you think there could be problems? In this…
Hi,
Is it possible to generate isolated -12V output from +12V input using LTM8048? I couldn't find such application information in the datasheet or demo board. do you see any potential issue with the schematic below? please advise. Thanks.
Rega…
原本做光学,2015年因工作内容需要学习电子行业的相关知识,从系统单机的电源模块开始,现在还带着LTM8048的一个问题尚未解决,然后ADC、DAC芯片,其间无数次的翻ADI的技术讨论文档,解决心中的疑问,不断的在疑惑、解疑的循环中学习知识,今天我又带着高速比较器的一些疑问来翻阅ADI的技术文档,恰巧看到通知里模拟对话50周年(工作原因平时只能用手机针对性的查阅资料,不登录自己的账号),已经电子订阅!期待一份纸质版的放在工位上。生快~
LTM8045 |
LTM8049 |
LTM4651 |
LTM4661 |
LTM4686 |
LTM4676 |
LTM4686-1 |
LTM4676A |
LTM4675 |
LTM4677 |
LTM4678 |
LTM8062 |
LTM8061 |
LTM8052 |
LTM8026 |
LTM8056 |
LTM8064 |
LTM8054 |
LTM8055 |
LTM4600 |
LTM4600HV |
LTM4608A |
LTM4604A |
LTM8032 |