• LTM8046 Continuous working voltage

    Hi,

    We are looking to use the LTM8046 to provide an isolation barrier with a 500V DC working voltage. We are happy that there is sufficient clearance and creepage at the device pins. The datasheet says the device is hi-pot tested at 3kV for 1 second but…

  • LTM8046 input voltage range vs output voltage

    Hello,

    I want to convert 28V input to 5V,450mA isolated output by using LTM8046 . In datasheet, says LTM8046 maximum input is 31V .  However, DC1559A demo board specifies input range maximum 26V, also in datasheet circuits.

    Is the input maximum voltage…

  • LTM8046 gnd isolation

    Hi,

    I want to use LTM8046 in my application. My application doesn't need isolation requirement. So can I short i/p and o/p GND pins of LTM8046.

    Please clarify.

    Amit

  • Isolated DC-DC converter for Lithium Ion battery operated application

    Hi There,

    I need to use a Isolated DC to DC converter which will have an input of 3.7V Lithium Ion battery and output should be 3.3V. I was looking at LTM8046, But the input voltage range does not match. Can you please suggest a part for same application…

  • RE: What the key difference between LMT8057 and LMT8046

    The LTM8046 has higher output power capability, i.e. 5Vout at 550mA at 24Vin vs 5Vout at 330mA at 24Vin for the LTM8057.

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • 官方资料上线丨《数字隔离和接口技术选型指南2021》免费下载ing~

    “数字化”正在全球范围内掀起浪潮,推动科技如闪电般速度发展:数字医疗健康、电动汽车、 5G通信和智能制造……
    电子化器件中离不开隔离技术,而数字隔离凭借其更低的噪声和电磁干扰、更高的安全性以及更长的使用寿命,是隔离发展的必然趋势。
    ADI在数字隔离技术方面有着丰富的经验,iCoupler数字隔离可保护人员和财产免受高压影响,并保护关键数据免受破坏性电干扰。
    那么面对不同的应用领域,如何选择适合的数字隔离和接口解决方案以最大化加速您的项目?

    AD…