• LTM4700使用问题

    您好,

    使用LTM4700遇到一个问题:在负载不满载时,没有问题,负载满载时(电流约60A),运行一段时间电源会掉电一下,怀疑是过流导致电源保护,环路补偿设置不合适,但是环路补偿如何设置一个最佳值呢?

  • Vout of LTM4700 before writing EEPROM

    Hello,

    I'm a DFAE in Japan. Our customer designs the schematic including LTM4700. If power is supplied to Vin of LTM4700 before writing the setting value of EEPROM, will 0V be output from Vout?

    Since the LTM4700 supplies power to the FPGA, he is concerned…

  • How to choose LTM4700 RVOUT resistors

    In my design the output of LTM4700 should be 0.85V@100A, but I cannot find Rvout_cfg and RVtrim_cfg Resistors setting in the datasheet.

    Could you please help to give the guide?

    Thanks in advance.

  • LTM4700两片并联使用

    您好,我现在在使用两片LTM4700并联输出0.9V@200A,但是芯片无法正常工作,芯片输出0.9V大概0.2ms后拉低,0.8ms后输出0.9V(此时芯片一直有响声,频率和上述现象一致),拆除一片后,芯片正常输出;测量了一下SHARE_CLK,都是100KHz,幅度3.4V左右;这种情况下再继续怎么排查,还有哪里需要注意?

  • LTM4700, Can the two channels be used independently?

    It is mentioned in the manual that vin0 to vout0 and vin1 to Vout1 are tested independently. Therefore, in my design, the two inputs are not from the same source. There may be a scene where vin0 is 12V, but vin1 is 0V. Is there any problem with this design…

  • LTM4700 两路输入能否能独立?

    LTM4700手册中有提到,Vin0和Vin1是互相独立的。在我的应用中,Vin0和Vin1是两个独立的输入源,有可能存在只有Vin0有电压,而Vin1无输入,这样设计是否会有问题?

    手册中提到的应用场景中,似乎都没有关于这一点的。所以我想要确认一下,谢谢。

  • LTM4700单片使用,一个通道工作正常,另外一个没有任何输出。

    LTM4700单片使用,一个通道工作正常,另外一个没有任何输出,两通道的配置相同,调整外部的环路参数也没反应,请问有什么办法分析?或是有没有其他客户遇到此类问题,谢谢。

  • 转换器LTM4700 的资料上为什么marking finish code是e4,下面的芯片上显示e1?

    LTM4700 的资料上为什么marking finish code是e4,下面的芯片上显示e1?

  • RE: 4款硬核产品、5大年度最佳,ADI角逐2019全球电子成就奖!

    年度电源管理/电压转换器  LTM4700

    产品详情:https://www.analog.com/cn/products/ltm4700.html

    LTM4700是一款双路 50A 或单路 100A 降压型 μModule DC/DC稳压器。通过采用创新的散热封装技术,ADI公司将LTM4700 的工作温度控制在仅 73°C左右,其它竞争产品的模块化解决方案运行温度则通常为 90°C。即使在高达 70°C 的环境温度中,只要辅以 200 LFM 气流散热,LTM4700 即可在 12VIN 至 0…

  • RE: LTM4675 test GUI for LTpowerPlay

    LTM4700 is a single 100A module and see if it can match your design.

    https://www.analog.com/en/products/ltm4700.html

    Thanks