• RE: LTM4691 step model

    Yes.

    The 3D steps file can be found under Design Resources --> Symbols and Footprints

  • LTM4691 high output ripple

    Hello Colleagues,

    I've noticed that the LTM4691 SPICE model sometimes runs at 1/2 switching frequency, higher than normal output ripple, and subharmonics at 1/8 the switching frequency. This usually happens when the output current exceeds 1A (the LTM4691…

  • LTM4691 Footprint Support to Allegro Library

    Dear All:

    LTM4691 Symbols and Footprints downloaded on the ADI website all support the PADS system, can you provide me with Allegro Library files? thanks

    Best

    Jack

  • RE: 有奖活动丨这次,跟着ADI一起成为“追光者”,看遍光电新趋势!

    双通道2A输出电源模组-LTM4691

    除了光通信控制器的展示外,现场还配套展示了LTM4691这一款高效率、双路输出降压型µModule降压稳压器,能够通过2.25 V至3.6 V输入电压为每通道提供2A连续输出电流。此开关模式电源采用3mm × 4mm × 1.18mm小型LGA封装,其中包含开关控制器、功率FET、电感和所有支持元件。每个输出可通过电阻独立设置的可编程电压范围为0.5 V至2.5 V。

  • Go Small or Go Home

    Today’s story is how the road to success required Analog Devices to think smaller.

    As I type this blog it is exactly 23 years – June 2, 1997 – since I began my career at ADI. I can hear my 1997 self asking “Blog? What’s a blog?” Sure, there was…

  • RE: ADI uModule PCB Footprint Library

    Hi Jack,

    Can you share more details how important this request is "from Pads to Allegro" moving forward? I'm aware that there is a converter to Allegro using PADS or Altium that customer can do. Is this something customer cannot do?

    About your…

  • ADI最近有哪些重点产品?ADC、ISO、Power、RF...都在这里了

    天气越来越冷,它们却火热到不行~

    今天,斑竹为大家带来了近期ADI 5款热门器件的盘点~

    快来瞧一瞧,看一看鸭~

    同步采样ADC AD7134

    AD7134 是一款四通道、低噪声、同步采样、精密模数转换器 (ADC),具备功能性、高性能和易用性。AD7134 基于连续时间 Σ-Δ (CTSD) 调制方案,使得 Σ-Δ 调制器前面不再需要传统上必需的开关电容电路采样,因而放宽了 ADC 输入驱动要求。CTSD 架构还可固有地抑制 ADC 混叠频带周围的信号,使套件具有固有的抗混叠能力,同时不再需要复杂的外部抗混叠滤波器…

  • 在新年到来之际,送你一组钻石级硬度的精选硬核产品吧~

    转眼间,2020年就要结束了,今年你都做了些什么呢?

    对于ADI,我们可是推出了不少硬核产品哦~

    今天,斑竹就给大家晒晒ADI这些杠杠滴成果!

    -------------------------------------------------------------------------

    软件可配置的四通道输入/输出 AD74413R

    AD74413R是一款软件可配置的四通道输入/输出解决方案,适用于楼宇和过程控制应用。AD74413R包含用于模拟输出、模拟输入、数字输入、电阻温度检测器(RTD…

  • ADI 全新中文资料(2020 年 9 月)