Hi
I am looking for the drawing of LTM4678's tray.
Which is correct drawing 50-8083 or 50-8078?
If the other is correct, could you please send it?
Best regards
N.Kokubo
PDFPDF
Hello,
Where can I find details on bulk programming of the LTM4678 internal EEPROM?
Downloading the schematic symbol from:
https://www.analog.com/media/en/symbols-footprints/symbols/LTM4678_footprints_symbols.zip
I get an OrCad symbol that does not match the DC2552A demo board schematic, and appears to have the following mistakes:
Pin…
I have a board design using two LTM4678 devices.
I am working with the DC2552A dev board for the LTM4678 device. It is preset for 1.8 and 1.0 outputs. I have the DC1613A attached. Both operate as expected with no-load. The 1.8V supply functions from no…
hi, I want to download the model of LTM4678 PARALLEL,but the link can't be used on the ADI site.Where can I down the model from?
When I program my LTM4678 outputs to +2.0V, I get a sensible small current from my open-circuit load. When I then program it to >= +2.1V, suddenly it says it is drawing > 2.5A, which can't be correct for a small linear step and no load. Changing…
Dear All
I'm Lonnie Kim DFAE at Sheenbang in Korea.
Our customer wants to LTM4678 100A parallel model.
Where can I get that model's data?
Lonnie Kim(sykim@sheenbang.com)
Greetings,
For part re-use I would like to bypass INTVCC with the same 4.7uF ceramic cap as EXTVCC, but the datasheet calls out 2.2uF. Is this exact value needed to e.g. run an ADC, or is anything in the range of 2.2uF OK? Thanks!
發現日期
問題內容
不良圖片
目前處理方式
長期解決方式
負責單位
目前狀態
2020.12.11
LTM4678物料表面不平整,無法使用公規吸嘴進行作業
使用高溫膠帶貼附表面使用公規吸嘴置件
與供應商協調來料協助貼附黃色高溫膠帶
PM
OPEN
需求:12v输入,初始电压1.0v,上电之后通过PMBUS改为0.85v,电流150A;
当前设计:
1、三个LTM4678电源模块并联实现,上电初始电压1.0v,上电完成之后要求通过PMBUS接口改成0.85v,但是在修改过程中,3个模块电压不可能同时修改成0.85v,肯定有先后顺序。如果第一个模块电压改为0.85v,但是余下两个模块的电压还没有改过来,这个是否有影响?是否有参考设计?
2、如果第一种方案不行,是否可以用1个ltm4678+2个LTM4650,这样是否可以使用?有没有参考设计?